RF Output Block

This topic describes the parameters of the RF Output block.

Important Information for Bonded Configurations

Unless specified as "Bonded," this topic primarily describes capabilities for use when the Configuration is Independent, 2 Tx Coherent, or MIMO. For bonded configurations, do not use SCPI commands described in this topic unless they are specified as "Bonded."

For bonded configurations, be sure to use bonding-supported SCPI commands only. Using unsupported SCPI commands in a bonded configuration will impair the fidelity of the waveform.  In these cases, the unsupported SCPI commands are still accepted, but no error or warning is generated.

General Settings Vary with VXG Models

Some RF Output settings in the General tab vary according to the signal generator model. Use the images below to see these differences. Use the table below to access descriptions for your model.

ClosedM9484C VXG (view image)

Tab

M9484C

Amplitude

RF Out (All)

Enable RF Output

RF Out (Bonded)

Power Mode

Power (Total RMS)

Power (Total RMS) (Bonded)

Power Increment

Impedance

Fast Power

Fast Frequency and Power

Peak Envelope Power

User Power Limit On/Off

User Power Limit

Attenuation Hold Mode

Attenuation Auto (Attenuation Hold)

ALC On

ALC - Auto

ALC - Edge Detection On

ALC - Bandwidth

ALC Level

ALC Source

Power Meter Servo

Channel

Device Name

Increment

User Power Maximum Limit

Settling Error

Initial Power

Until Delta

Channel Gain Overview

Channel Gain Power Headroom

Channel Gain Power Headroom Auto

Channel Gain Power Reference

Channel Gain Power Reference Auto

Amplitude Offset

Amplitude Reference On/Off

Amplitude Reference Value

Set Reference to Current Amplitude

Power Search

Frequency and Phase

RF Out (Bonded)

Frequency (CW)

Frequency (CW) (Bonded)

Frequency Increment

Frequency Increment (Bonded)

Fast Frequency

Phase Transition Mode

Phase

Phase Reference

Frequency Offset

Frequency Offset State

Frequency Multiplier

Frequency Reference On/Off

Frequency Reference Value

Set Reference to Current Frequency

Corrections/De-embedding - This link opens a separate topic.
Optimizations - This link opens a separate topic.
List/Step Sweep - This link opens a separate topic.

Frequency List/Sweep

Frequency Center (Remote command only)

Frequency Span (Remote command only)

Frequency Start

Frequency Stop

RF Out (All)

For multi-channel capability only.

Turns the RF outputs on or off for all the channels in the instrument. This is a master control that gates the individual states. If this control is off, no RF power is emitted from any of the channels; however, the individual channels retain the state of their setting. If this control is on, the RF outputs are on if their individual state is on. To enable or disable individual channels see RF Out.

GUI Location

RF Out (All)

SCPI Command

[:SOURce]:RFALl:OUTPut[:STATe] ON|OFF|1|0

[:SOURce]:RFALl:OUTPut[:STATe]?

SCPI Example

RFAL:OUTP OFF

RFAL:OUTP?

Preset

ON

State Saved

Yes

Choices

OFF | ON

Initial S/W Revision

A.01.00

Amplitude

Enable RF Output

Enables or disables the RF output of the indicated channel. To enable or disable all channels, see RF Out (All).

The state of RF Out (All) does not change the RF Out state of a specific channel. For example, if RF Out for Channel 1 is set to on and RF Out (All) is set to off, no power is emitted from the RF Output connector of Channel 1. Likewise, if RF Out for Channel 1 is set to off and RF Out (All) is set to on, no power is emitted from the RF Output connector of Channel 1.

Do not use these SCPI commands for channel bonding. While an error or warning is not generated in this case, the fidelity of the bonded waveform is impaired.

Instead, refer to RF Out (Bonded).

GUI Location

RF Out

SCPI Command

[:SOURce][:RF<channel>]:OUTPut[:STATe] ON|OFF|1|0

[:SOURce][:RF<channel>]:OUTPut[:STATe]?

SCPI Example

OUTP ON

OUTP?

Notes

If the M9484APPC or M9484AP1C license is not installed, attempting to set state to ON generates an application error message.

The state of Global RF does not change the state of the per-channel RF; e.g. if SOUR:RF1:OUTP is ON and SOUR:RFAL:OUTP is OFF, no power is emitted from the RF Output connector of Channel 1; and if SOUR:RF1:OUTP is OFF and SOUR:RFAL:OUTP is set to ON, no power is emitted from the RF Output connector of Channel 1.

Preset

OFF

State Saved

Yes

Choices

OFF | ON

Initial S/W Revision

A.01.00

History

Added M9484APPC or M9484AP1C at A.09.00

RF Out (Bonded)

Enables or disables the RF output of all physical channels in the bonded set. To enable or disable all channels see RF Out (All).

GUI Location

System Menu > Configure Channels > 2 Channel Bonded > RF Out (bonded-channel icon)

SCPI Command

[:SOURce]:GROup<group>:CBONded:OUTPut[:STATe] ON|OFF|1|0

[:SOURce]:GROup<group>:CBONded:OUTPut[:STATe]?

SCPI Example

GRO:CBON:OUTP OFF

GRO:CBON:OUTP?

Preset

OFF

State Saved

Yes

Range

OFF | ON

SCPI Change

[:SOURce]:CBONded<bondingset>:OUTPut[:STATe] ON|OFF|1|0 has been changed to [:SOURce]:GROup<group>:CBONded:OUTPut[:STATe] ON|OFF|1|0.

Prior use of :SOUR:CBON:OUTP or :SOUR:CBON1:OUTP is now :SOUR:GRO1:CBON:OUTP.

Initial S/W Revision

A.07.00

Modified S/W Revision

A.10.00 Changed SCPI: Added GROup<group> and removed <bondingset> from :CBONded

Power Mode

Remote command only.

Sets the power mode of the indicated channel.

SCPI Command

[:SOURce][:RF<channel>]:POWer:MODE FIXed|LIST

[:SOURce][:RF<channel>]:POWer:MODE?

SCPI Example

POW:MODE LIST

POW:MODE?

Couplings
  • When List/Step Sweep State is ON and Power Sweep State is set to OFF, Power Mode is set to Fixed.

  • When List/Step Sweep State is ON and Power Sweep State is set to ON, Power Mode is set to List.

  • When List/Step Sweep State is OFF, Power Mode is set to Fixed.

Preset

FIX

State Saved

Yes

Choices Fixed | List
Backward Compatibility SCPI

N5182B:

[:SOURce]:POWer:MODE

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:POWer:MODE SWEep to

[:SOURce]:RF1:POWer :MODE LIST

Alias [:SOURce][:RF<channel>]:POWer:MODE SWEep to

[:SOURce][:RF<channel>]:POWer :MODE LIST

Initial S/W Revision

A.16.00

Power (Total RMS)

Controls the RF output power of the indicated channel.

This is the value that the instrument attempts to output. The actual value might be different from the specified value due to the hardware limitations. For example, the output power is different when a high power value is specified with Attenuation Auto off (that is, Attenuation Hold on).

When Power Sweep State is ON, changing the power sets the Power Sweep State to OFF.

GUI Location

RF Output > Amplitude tab > Power (Total RMS)

SCPI Command

[:SOURce][:RF<channel>]:POWer[:LEVel][:IMMediate][:AMPLitude] <ampl>

[:SOURce][:RF<channel>]:POWer[:LEVel][:IMMediate][:AMPLitude]?

SCPI Example

POW -50

POW?

Couplings

For M9484C with Option 8SG:

  • When Absolute Power Mode is ON, the sum of enabled signals’ Absolute Powers is set to the RF Channel’s Output Power. If the RF Channel Output Power is changed, then all enabled signals are adjusted, maintaining the relative relationship between them specified by the signals’ Relative Powers.

Notes

The maximum value of this setting is a settable maximum and the datasheet describes actual specified max power that the instruments are capable of.

Dependencies

When the power is clipped to the User Power Limit the error message "Clipped to User Power Limit" is displayed on the GUI or -222; "Data out of range; Clipped to User Power Limit" to SCPI.

Preset

-100 dBm

When SCPI Backward Compatibility Mode is N51xxB:

  • For Channel 1: Min

State Saved

Yes

Min

-135 dBm

Max

For M9484C:

  • With Option 1EA: 30 dBm

  • WithOption 1EB: 30 dBm

  • WithOption 1EC: 30 dBm

  • With Option 1EE: 30 dBm from 9 kHz to 43.5 GHz, 18 dBm above 43.5 GHz

  • Otherwise: 20 dBm

Resolution

0.01 dBm

Initial S/W Revision

A.01.00

Modified S/W Revision

A.09.00, A.10.00

History

The preset value was changed from -120 dBm at A.03.00 since ALC shows an error with -120 dBm on 20 GHz box.

Updated Max at A.03.00.

Updated Max at A.09.00.

Updated Max for M9484C from 18 dBm to 20 dBm for standard power in A.10.00.

Power List / Step Sweep

Refer to the sections Power Start and Power Stop in Step Sweep Configuration.

Power (Total RMS) (Bonded)

Sets the power into the Device Under Test, the signal at the output of the external combiner. The power calibration, as part of the bonding process, must be performed in order to achieve the specified power level at the output of the combiner. Otherwise the actual power will be reduced by the cable loss and loss through the combiner.

The actual output power available is dependent on the instrument’s output capability and cable and fixture losses.

GUI Location

System Menu > Configure Channels > Bonded > Power (entry field)

SCPI Command

[:SOURce]:GROup<group>:CBONded:POWer[:LEVel][:IMMediate][:AMPLitude] <ampl>

[:SOURce]:GROup<group>:CBONded:POWer[:LEVel][:IMMediate][:AMPLitude]?

SCPI Example

GRO:CBON:POW 0

GRO:CBON:POW?

Notes

The maximum value of this setting is a settable maximum and the data sheet describes the actual specified max power that the instruments are capable of.

Dependencies

When the power is clipped to the User Power Limit the error message "Clipped to User Power Limit" is displayed on the GUI or -222;"Data out of range;Clipped to User Power Limit" to SCPI.

Preset

-100 dBm

State Saved

Yes

Min

-120 dBm

Max

For M9484C: 21 dBm in all frequencies not covered by these options:

  • With Option 1EA: 33 dBm

  • With Option 1EB: 33 dBm

  • With Option 1EC: 33 dBm

  • With Option 1EE: 33 dBm from 9 kHz to 43.5 GHz, 21 dBm above 43.5 GHz

Resolution

0.01 dBm

SCPI Change

[:SOURce]:CBONded<bondingset>:POWer[:LEVel][:IMMediate][:AMPLitude] <ampl> has been changed to [:SOURce]:GROup<group>:CBONded:POWer[:LEVel][:IMMediate][:AMPLitude] <ampl>.

Prior use of :SOUR:CBON:POW or :SOUR:CBON1:POW is now :SOUR:GRO1:CBON:POW.

Initial S/W Revision

A.07.00

Modified S/W Revision

A.10.00 Changed SCPI: Added GROup<group> and removed <bondingset> from :CBONded

Power Increment

Remote command only.

Controls the incremental step value of the RF output power for the specified channel.

SCPI Command

[:SOURce][:RF<channel>]:POWer[:LEVel][:IMMediate][:AMPLitude]:STEP[:INCRement] <ampl>

[:SOURce][:RF<channel>]:POWer[:LEVel][:IMMediate][:AMPLitude]:STEP[:INCRement]? [MAXimum|MINimum]

SCPI Example

POW:STEP 10

POW:STEP?

Preset 1 dBm

Notes

 

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Min

0.01 dBm

Max

100 dBm

Resolution

0.01 dBm

Initial S/W Revision

A.20.00

Impedance

Remote command only.

Query only. Provided to allow programmatic compatibility with SMA100x signal generators.

SCPI Command

[:SOURce][:RF<channel>]:OUTPut:IMPedance?

SCPI Example

:OUTP:IMP?

Initial S/W Revision

A.20.00

Fast Power

Remote command only.

Sets the instrument’s power with the maximum throughput.  As the purpose of this command is for speed, there is no limit checking, no coupling, and no update of the value on the front panel.  When using this command, there is no inclusion of amplitude offset or amplitude reference. The value is a floating point number in dBm.  No error message is raised if the value is clipped.

SCPI Command

FAST<channel>:POWer <double>

SCPI Example

FAST:POW -50

Notes

This command performs no coupling, does not support UP, DOWN, MIN, MAX, DEF.  The value is floating point value in dBm; no DB or DBM units are allowed.

State Saved

No

Min

-135.0

Max

For M9484C:

  • With Option 1EA: 30.0

  • With Option 1EB: 30.0

  • With Option 1EC: 30.0

  • With Option 1EE: 30.0 from 9 kHz to 43.5 GHz, 18.0 above 43.5 GHz

  • Otherwise: 20.0

Resolution

0.01

Initial S/W Revision

A.14.00

Fast Frequency and Power

Remote command only.

Sets the instrument’s frequency and power with the maximum throughput. As the purpose of this command is for speed, there is no limit checking, no coupling, and no update of the value on the front panel.  When using this command, there is no inclusion of frequency offset, multiplier, frequency reference, amplitude offset, or amplitude reference.  The value is an integer frequency in 10 uHz resolution.  No error message is raised if the value is clipped.

SCPI Command

FAST<channel>:FP <integer>,<double>

SCPI Example

FAST:FP 300000000000000,-50

Notes

This command performs no coupling, does not support UP, DOWN, MIN, MAX, DEF.  The frequency value is an integer in 10 uHz, power value is a double in dBm; no HZ, KHZ, MHZ, GHZ, DB, DBM units are allowed.

See Fast Frequency section for details of the frequency setting and Fast Powersection for details of the power setting.

State Saved

No

Initial S/W Revision

A.14.00

Peak Envelope Power

Displays or returns the peak envelope power.

GUI Location

RF Output > Amplitude tab > Peak Envelope Power

SCPI Command

[:SOURce][:RF<channel>]:POWer:PEPower?

SCPI Example

POW:PEP?

Initial S/W Revision

A.01.00

User Power Limit On/Off

Enables the maximum output power limit set by User Power Limit of the indicated channel.

The value set with this command is not affected by *RST or a power cycle. It is reset to default value with Restore System Defaults.

GUI Location

RF Output > Amplitude tab > User Power Limit

SCPI Command

[:SOURce][:RF<channel>]:POWer:USER:ENABle ON|OFF|1|0

[:SOURce][:RF<channel>]:POWer:USER:ENABle?

SCPI Example

POW:USER:ENAB ON

POW:USER:ENAB?

Preset

This is unaffected by a Preset but is set to OFF on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Initial S/W Revision

A.01.00

User Power Limit

Sets the maximum output power level for the indicated channel that is lower than the instrument’s normal maximum output power. This affects all modes of power operation. This affects the Amplitude value, but features such as AM may allow the power to exceed the Amplitude value. In other words, this is not a hardware power clamp. 

The value is not affected by recall, *RST, Preset or a power-cycle. It is reset to the default value with Restore System Defaults.

GUI Location

RF Output > Amplitude tab > User Power Limit

SCPI Command

[:SOURce][:RF<channel>]:POWer:USER:MAXimum <ampl>

[:SOURce][:RF<channel>]:POWer:USER:MAXimum?

SCPI Example

POW:USER:MAX 10

POW:USER:MAX?

Dependencies

Default value of 0 dBm is set by Restore System Defaults

Preset

0 dBm

State Saved

No

Min

-135 dBm

Max

30 dBm

Resolution

0.01 dBm

Initial S/W Revision

A.01.00

Attenuation Hold Mode

Enabling attenuation hold (Hold checkbox is marked in the GUI) turns off automatic attenuation and allows you to select one of the following possible RF Output behaviors in the Attenuation Hold Mode drop-down menu.

Attenuation Hold Mode

Description

Summary

Output

Holds only the output attenuators but allows non-output attenuators to change. Output attenuators are defined as those that, when changed, affect the source match and have the potential to introduce some discontinuity on power changes when not held. They are also distinct in that they are selected based on mode, requested power and frequency only and have no dependency on signal level coming from the DAC. Changing non-output attenuation can result in small discontinuities.

  • Power Reference Auto is overridden to off

  • Changing RF Power may change non-output attenuators

  • Changing Power Reference will change attenuators

  • Changing the Power Headroom will not change output attenuators

  • Note: depending on the hardware, holding output attenuators can be enough to avoid any power discontinuities, but only with ALC or some other form of power correction on.

All

Holds all attenuators, avoiding all attenuation-based discontinuities at the cost of dynamic range.

  • Power Reference Auto is overridden to off

  • Changing RF Power will not change any attenuators

  • Changing Power Reference will change attenuators

  • RF Power adjustment range is "excess" headroom for higher power, as it is consuming the digital scale.

  • Changing the Power Headroom can change attenuators

GUI Location

RF Output > Amplitude tab > Attenuation Hold Mode

SCPI Command

[:SOURce][:RF<channel>]:POWer:ATTenuation:HOLD:MODE OUTPut|ALL

[:SOURce][:RF<channel>]:POWer:ATTenuation:HOLD:MODE?

SCPI Example

POW:ATT:HOLD:MODE ALL

POW:ATT:HOLD:MODE?

Preset

OUTPut

Range

For M9484C

Output|All

State Saved

Y

Initial S/W Revision

A.12.00

Attenuation Auto (Attenuation Hold)

Turns the output Attenuator Hold function off or on. When Hold is off (checkbox cleared), auto attenuation is on; when Hold is on, auto attenuation is off. The GUI enables or disables the Hold function, while the SCPI command enables or disables the Auto function. In other words, the GUI and SCPI selections achieve the same result with opposite settings, as outlined in the table below.

GUI

SCPI

Description

POW:ATT:AUTO ON

The attenuator setting is automatically changed as needed to maintain the RF output power level.

  • Attenuation Hold is Off

  • Attenuation Auto is On

  • Power Reference Auto is under user control

  • See Attenuation Hold Mode for details

 

POW:ATT:AUTO OFF

The attenuator remains at its current setting.

  • Attenuation Hold is On

  • Attenuation Auto is Off

  • Channel Gain Power Reference Auto to is overridden to Off.

  • See Attenuation Hold Mode for details.

You can use the Attenuation Hold function to eliminate power level transients that can occur with attenuator switching.

When Attenuation Hold is turned on with User Power Limit on, the output power may exceed the specified power limit because the specified attenuation may not be high enough to achieve the power limit.

GUI Location

RF Output > Amplitude tab > Attenuation [or Attenuation Hold Mode] > Hold

SCPI Command

[:SOURce][:RF<channel>]:POWer:ATTenuation:AUTO ON|OFF|1|0

[:SOURce][:RF<channel>]:POWer:ATTenuation:AUTO?

SCPI Example

POW:ATT:AUTO OFF

POW:ATT:AUTO?

Notes

For M9484C:

Attenuation Auto is On and is not changeable (however, sending the SCPI command does not generate an error.)

Preset (SCPI)

ON (Attenuation Auto)

Preset (GUI)

OFF (Attenuation Hold)

State Saved

Yes

Choices

OFF | ON

Initial S/W Revision

A.01.00

ALC On

Enables or disables the automatic leveling control (ALC) circuit on the indicated channel. The purpose of the ALC circuit is to hold output power at a desired level by adjusting the instrument’s power circuits for power drift. Power will drift over time and with changes in temperature.

GUI Location

RF Output > Amplitude tab > ALC On

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC[:STATe] ON|OFF|1|0

[:SOURce][:RF<channel>]:POWer:ALC[:STATe]?

SCPI Example

POW:ALC OFF

POW:ALC?

Choices

OFF | ON

Couplings

When ALC Auto is on, ALC On/Off changes as follows:

  • ALC On/Off becomes off when:

    • the frequency is less than 10 MHz

    • or the frequency is greater than 40 GHz

    • or Vector Modulation of any signal is ON

    • or I/Q Modulation is ON with no signal enabled

  • Otherwise: ALC becomes ON

Preset

ON

When SCPI Backward Compatibility Mode is N51xxB and Suppress SCPI Compatibility Errors is ON:

  • For Channel 1: ON

State Saved

Yes

Initial S/W Revision

A.01.00

Modified at S/W Revision A.20.01 - Added coupling: ALC becomes Off when I/Q Modulation is On with no signal enabled

ALC - Auto

Enables or disables ALC On and ALC - Bandwidth couplings. Setting ALC On or ALC Bandwidth turns this parameter off.

For IQ modulation, the ALC & Power Search should always be set to Auto.

Coupling conditions are described in ALC On and ALC - Bandwidth.

GUI Location

RF Output > Amplitude tab > ALC Auto

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:AUTO ON|OFF|1|0

[:SOURce][:RF<channel>]:POWer:ALC:AUTO?

SCPI Example

POW:ALC:AUTO OFF

POW:ALC:AUTO?

Preset

ON

State Saved

Yes

Choices

OFF | ON

Initial S/W Revision

A.01.00

ALC - Edge Detection On

Enables or disables the ALC ignoring pulse edges. When steep slopes are detected in the magnitude, the ALC ignores a small time-window around the steep slope. This allows leveling on only the center portion of pulses and not the edges. If this feature is on, and the signal is not pulsed with a high crest factor, the ALC will intermittently ignore samples, effectively lowering the BW of the ALC loop.

GUI Location

RF Output > Amplitude tab >  Edge Detection On

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:EDETect[:STATe] ON|OFF|1|0

[:SOURce][:RF<channel>]:POWer:ALC:EDETect[:STATe]?

SCPI Example

POW:ALC:EDET OFF

POW:ALC:EDET?

Preset

ON

State Saved

Yes

Choices

OFF | ON

Initial S/W Revision

A.09.00

ALC - Bandwidth

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

For IQ modulation, the ALC and Power Search should always be set to Auto.

GUI Location

RF Output > Amplitude tab > Bandwidth

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:BANDwidth VSLow|SLOW|MEDium|FAST

[:SOURce][:RF<channel>]:POWer:ALC:BANDwidth?

SCPI Example

POW:ALC:BAND MED

POW:ALC:BAND?

Notes

ALC Bandwidth is VSLow and not changeable, sending the SCPI command does not generate an error.

Preset

Very Slow

State Saved

Yes

Choices

Very Slow

Initial S/W Revision

A.01.00

The table below shows some of the ALC Bandwidth coupling examples.

ALC Level

Remote command only.

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:LEVel <ampl>

[:SOURce][:RF<channel>]:POWer:ALC:LEVel?

SCPI Example

POW:ALC:LEV 5 dBm

POW:ALC:LEV?

Notes

Level is -20 dBm and not changeable, sending the SCPI command does not generate an error.

Preset

-20 dBm

When SCPI Backward Compatibility Mode is N51xxB:

  • For Channel 1: 1 dBm

State Saved

Yes

Min

-20 dBm

Max

-20 dBm

Resolution

0.01

Step

0.01

Backwards Compatibility

[:SOURce]:POWer:ALC:LEVel

Initial S/W Revision

A.04.00

ALC Source

Remote command only.

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SOURce INTernal

[:SOURce][:RF<channel>]:POWer:ALC:SOURce?

SCPI Example

PPOW:ALC:SOUR INT

POW:ALC:SOUR?

Notes

This command is accepted and does not raise an error.

For N51xxB compatibility, PMONce and PMContinuous are accepted and activate Power Meter Servo. See Backwards Compatibility Notes in this table.

Preset

INT

Range

INT

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:POWer:ALC:SOURce

Backwards Compatibility Notes

For N51xxB:

  • When INTernal|DIODe is set, if Power Meter Servo is running, it is stopped. DIODe is not supported.

  • When PMONce|PMContinuous is set, Power Meter Servo is run. The power meter device must first be registered in the Device List using the name specified in the Device Name setting. See Power Meter Servo.

State Saved

Yes

Initial S/W Revision

A.04.00

Modified at S/W Revision A.20.00 - Added N51xxB Backwards Compatibility

Power Meter Servo

Uses power meter readings to adjust the output power of the source, maintaining a constant DUT output power. The servo loop measures the output power of the DUT, compares it to the user-provided reference power, and adjusts the output of the source to achieve the user-provided power level within the Settling Error.

This feature is activated through N51xxB backwards compatible commands only. See ALC Source.

Channel

Remote command only

Sets the power meter channel used for servo leveling.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:CHANnel A|B

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:CHANnel?

SCPI Example

POW:ALC:SOUR:PMS:CHAN B

POW:ALC:SOUR:PMS:CHAN?

Preset A
Range A|B
State Saved Yes
Backwards Compatibility SCPI

N51xxB:

[:SOURce]:POWer:ALC:SOURce:PMServo:CHANnel

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:POWer:ALC:SOURce:PMServo:CHANnel to [:SOURce]:RF1:POWer:ALC:SOURce:PMServo:CHANnel.

Initial S/W Revision A.20.00

Device Name

Remote command only

Sets the Device List name of the power meter to use for Power Meter Servo leveling.

SCPI Command

[:SOURce][:RF<channel>]:POWer:PMServo:DEVice <string>

[:SOURce][:RF<channel>]:POWer:PMServo:DEVice?

SCPI Example

POW:PMS:DEV "MyPowerMeter"

POW:PMS:DEV?

Preset ""
State Saved Yes
Initial S/W Revision A.20.00

Increment

Remote command only

Sets the percentage of the measured power error applied per iteration in Power Meter Servo mode. The default of 100% applies the full measured error each cycle. Reducing this value prevents overshoot at the cost of additional measurement/adjustment cycles. Works in conjunction with Initial Power and Until Delta.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:INCRement <real>

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:INCRement?

SCPI Example

POW:ALC:SOUR:PMS:INCR 75

POW:ALC:SOUR:PMS:INCR?

Preset 100
Min 10
Max 100
Resolution 0.01
Step Increment 0.01
State Saved Yes
Backwards Compatibility SCPI

N51xxB:

[:SOURce]:POWer:ALC:SOURce:PMServo:INCRement

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:POWer:ALC:SOURce:PMServo:INCRement to [:SOURce]:RF1:POWer:ALC:SOURce:PMServo:INCRement.

Initial S/W Revision A.20.00

User Power Maximum Limit

Remote command only

Sets an RF output power protection limit during Power Meter Servo mode. The instrument restricts the output power to this value and shows UNLEVELED if the desired output power exceeds it.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:MAXimum <ampl>

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:MAXimum?

SCPI Example

POW:ALC:SOUR:PMS:MAX 10 dBm

POW:ALC:SOUR:PMS:MAX?

Preset 30 dBm
Min

Option dependent.

See M9484C Data Sheet

Max

Option dependent.

See M9484C Data Sheet

Resolution 0.01 dBm
Step Increment 0.01 dBm
State Saved Yes
Backwards Compatibility SCPI

N51xxB:

[:SOURce]:POWer:ALC:SOURce:PMServo:MAXimum

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:POWer:ALC:SOURce:PMServo:MAXimum to [:SOURce]:RF1:POWer:ALC:SOURce:PMServo:MAXimum.

Initial S/W Revision A.20.00

Settling Error

Remote command only

Sets the convergence threshold for Power Meter Servo mode. Measurement/adjustment cycles continue until the measured power error falls within this value.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:SERRor <rel_ampl>

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:SERRor?

SCPI Example

POW:ALC:SOUR:PMS:SERR 0.2 dB

POW:ALC:SOUR:PMS:SERR?

Preset 0.2 dB
Min 0.02 dB
Max 10 dB
Resolution 0.01 dB
Step Increment 0.01 dB
State Saved Yes
Backwards Compatibility SCPI

N51xxB:

[:SOURce]:POWer:ALC:SOURce:PMServo:SERRor

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:POWer:ALC:SOURce:PMServo:SERRor to [:SOURce]:RF1:POWer:ALC:SOURce:PMServo:SERRor.

Initial S/W Revision A.20.00

Initial Power

Remote command only

Sets a relative power offset below the target at which Power Meter Servo mode begins its measurement/adjustment cycles. The default of 0 dB starts from the instrument’s best power estimate; a negative value provides a safe-margin to prevent device overshoot when the configured offset is incorrect. Works in conjunction with Increment and Until Delta.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:STARt <rel_ampl>

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:STARt?

SCPI Example

POW:ALC:SOUR:PMS:STAR -3 dB

POW:ALC:SOUR:PMS:STAR?

Preset 0 dB
Min -50 dB
Max 0 dB
Resolution 0.01 dB
Step Increment 0.01 dB
State Saved Yes
Backwards Compatibility SCPI

N51xxB:

[:SOURce]:POWer:ALC:SOURce:PMServo:STARt

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:POWer:ALC:SOURce:PMServo:STARt to [:SOURce]:RF1:POWer:ALC:SOURce:PMServo:STARt.

Initial S/W Revision A.20.00

Until Delta

Remote command only

Sets the power error below which the servo bypasses the Increment percentage and applies the full remaining correction in a single step. While the measured error exceeds Until Delta, each cycle applies only the configured Increment fraction of the remaining error. Works in conjunction with Initial Power and Increment.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:STOP <rel_ampl>

[:SOURce][:RF<channel>]:POWer:ALC:SOURce:PMServo:STOP?

SCPI Example

POW:ALC:SOUR:PMS:STOP 3 dB

POW:ALC:SOUR:PMS:STOP?

Preset 1 dB
Min 0 dB
Max 50 dB
Resolution 0.1 dB
Step Increment 0.1 dB
State Saved Yes
Backwards Compatibility SCPI

N51xxB:

[:SOURce]:POWer:ALC:SOURce:PMServo:STOP

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:POWer:ALC:SOURce:PMServo:STOP to [:SOURce]:RF1:POWer:ALC:SOURce:PMServo:STOP.

Initial S/W Revision A.20.00

Channel Gain Overview

The Channel Gain is the instrument’s digital and analog setup to achieve a particular power with an input, such as a waveform.  There are two settings for the Channel Gain: Power Headroom and Power Reference.  See Figure: Determining Instrument’s Channel Gain Setup. When Channel Gain Power Headroom Auto is on, the Channel Gain Power Headroom is automatically set to the crest factor (after runtime scaling) of the waveform(s) being played.  When Channel Gain Power Reference Auto is on, the Channel Gain Power Reference is the RF Power.

Adjusting the power headroom or power reference allows for selecting a particular setup across a range of powers or for optimizations when the instrument does not know the best optimization point. These settings accomplish the same function as Attenuator Hold in other Keysight Technologies signal generators.

The channel gain power headroom must be at or above the total crest factor of all combined signals, including AWGN and CW interferers, to avoid a DAC overflow. When Auto is on, the system will set this value to the combined crest factors (after runtime scaling). The larger this value is, the less likely that summed signals will run out of power or have an arithmetic overflow, but less dynamic range will be available.

Diagram

Description automatically generated

Figure: Power Control with Multiple Signals

Diagram

Description automatically generated

Figure: Determining Instrument’s Channel Gain Setup

See Figure: Power Gain vs Signal Power to understand how a particular signal’s power relates to the static instrument setup set by the channel gain power settings.  The headroom sets the amount of digital back-off from full-scale CW.  The channel gain reference power Pref sets the optimized gain.  These two values determine the maximum peak power.  Digital Scale is the dynamic power control applied in the instrument’s DSP to get the appropriate power given the requested power of the signal to play and its crest factors.  The crest factors are determined implicitly for internally generated waveforms, or explicitly using the rms of the waveform(s).

Diagram, schematic

Description automatically generated

Figure: Power Gain vs Signal Power

Channel Gain Power Headroom

The reference headroom sets the amount of digital back-off from full-scale CW.  This value must be at or above the total crest factor of all combined signals to avoid overflow.  The larger this value is, the less likely that summed signals will run out of power or have an arithmetic overflow, but less dynamic range will be available. See Channel Gain Overview.

GUI Location

RF Output > Amplitude tab > Channel Gain Headroom

SCPI Command

[:SOURce][:RF<channel>]:POWer:CGAin:HEADroom <rel_ampl>

[:SOURce][:RF<channel>]:POWer:CGAin:HEADroom?

SCPI Example

POW:CGA:HEAD 10DB

POW:CGA:HEAD?

Notes

For values larger than 20 dB, the system may not be capable of delivering maximum specified power.

Dependencies

When this value is set, Channel Gain Power Headroom Auto is set to off.

Preset

0 dB

State Saved

Y

Min

0 dB

Max

100 dB

Resolution

0.01 dB

Initial S/W Revision

A.12.00

Channel Gain Power Headroom Auto

When in auto mode, the Power Headroom is the crest factor of the waveform(s) being played, if known.  When in CW mode (no modulation), the headroom is 0 dB. See Channel Gain Overview.

GUI Location

RF Output > Amplitude tab > Channel Gain Headroom Auto

SCPI Command

[:SOURce][:RF<channel>]:POWer:CGAin:HEADroom:AUTO ON|OFF|1|0

[:SOURce][:RF<channel>]:POWer:CGAin:HEADroom:AUTO?

SCPI Example

POW:CGA:HEAD:AUTO ON

POW:CGA:HEAD:AUTO?

Notes

When this feature is turned off, the automatic values are retained.

Preset

ON

State Saved

Yes

Initial S/W Revision

A.12.00

Channel Gain Power Reference

This value is the optimized power level for purposes of power control.  This follows RF Power when Auto is on. See Channel Gain Overview.

GUI Location

RF Output > Amplitude tab > Channel Gain Power Reference

SCPI Command

[:SOURce][:RF<channel>]:POWer:CGAin:REFerence <ampl>

[:SOURce][:RF<channel>]:POWer:CGAin:REFerence?

SCPI Example

POW:CGA:REF 0DBM

POW:CGA:REF?

Notes

The maximum value of this setting is a settable maximum and the datasheet describes actual specified max power that the instruments are capable of.

Dependencies

When the power is clipped to the User Power Limit the error message "Clipped to User Power Limit" is displayed on the GUI or -222;"Data out of range;Clipped to User Power Limit" to SCPI.

When this value is set, Channel Gain Power Reference Auto is set to off.

Preset

-100 dBm

State Saved

Yes

Min

-135 dBm

Max

For M9484C:

  • With Option 1EA: 30 dBm

  • With Option 1EB: 30 dBm

  • With Option 1EC: 30 dBm

  • With Option 1EE: 30 dBm from 9 kHz to 43.5 GHz, 18 dBm above 43.5 GHz

  • Otherwise: 20 dBm

Resolution

0.01 dBm

Initial S/W Revision

A.12.00

Channel Gain Power Reference Auto

When in auto mode, the Power Reference is the RF Power. See Channel Gain Overview.

GUI Location

RF Output > Amplitude tab > Channel Gain Power Reference Auto

SCPI Command

[:SOURce][:RF<channel>]:POWer:CGAin:REFerence:AUTO ON|OFF|1|0

[:SOURce][:RF<channel>]:POWer:CGAin:REFerence:AUTO?

SCPI Example

POW:CGA:REF:AUTO ON

POW:CGA:REF:AUTO?

Notes

When this feature is turned off, the automatic values are retained. 

Dependencies Can only be set to ON when Attenuation Auto is ON.

Preset

ON

State Saved

Yes

Initial S/W Revision

A.12.00

Amplitude Offset

Provides a power offset (in dB) to the actual RF output of the indicated channel. This simulates a power level at a test point beyond the RF OUTPUT connector without changing the actual RF output power. The offset value only affects the displayed amplitude setting. You can enter an offset at any time in either normal operation or amplitude reference mode.

GUI Location

RF Output > Amplitude tab > Amplitude Offset

SCPI Command

[:SOURce][:RF<channel>]:POWer[:LEVel][:IMMediate]:OFFSet <rel_ampl>

[:SOURce][:RF<channel>]:POWer[:LEVel][:IMMediate]:OFFSet? [MAXimum|MINimum]

SCPI Example

POW:OFFS 10 dB

POW:OFFS?

Preset

0 dB

State Saved

Yes

Range

-200 to 200 dB

Resolution

0.01 dB

Initial S/W Revision

A.01.00

Amplitude Reference On/Off

Enables or disables the amplitude reference mode for the indicated channel. When the amplitude reference mode is on, subsequent amplitude parameters are set relative to the reference value.

GUI Location

RF Output > Amplitude tab > Amplitude Reference

SCPI Command

[:SOURce][:RF<channel>]:POWer:REFerence:STATe ON|OFF|1|0

[:SOURce][:RF<channel>]:POWer:REFerence:STATe?

SCPI Example

POW:REF:STAT ON

POW:REF:STAT?

Preset

OFF

State Saved

Yes

Choices

OFF | ON

Initial S/W Revision

A.01.00

Amplitude Reference Value

Provides an amplitude reference value for the indicated channel.

GUI Location

RF Output > Amplitude tab > Amplitude Reference

SCPI Command

[:SOURce][:RF<channel>]:POWer:REFerence <ampl>

[:SOURce][:RF<channel>]:POWer:REFerence? [MAXimum|MINimum]

SCPI Example

POW:REF -20

POW:REF?

Preset

0 dBm

State Saved

Yes

Range

-330 to 220 dBm

Resolution

0.01 dBm

Initial S/W Revision

A.01.00

Set Reference to Current Amplitude

This immediate action sets the current output amplitude, along with any offset, as a 0 dBm reference value to the indicated channel.

GUI Location

RF Output > Amplitude tab > Set Reference to Current Amplitude

SCPI Command

[:SOURce][:RF<channel>]:POWer:REFerence:SET

SCPI Example

POW:REF:SET

Initial S/W Revision

A.01.00

Power Search

Other Keysight Technologies signal generators provided the ability to adjust the internal attenuators and amplifiers for coarse tuning and modulation scaling for fine tuning. The Power Search SCPI commands are provided to allow programmatic compatibility with those instruments.

Power Search Mode

Remote command only.

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. This command is accepted but does nothing.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SEARch ON|OFF|1|0|ONCE

[:SOURce][:RF<channel>]:POWer:ALC:SEARch?

SCPI Example

POW:ALC:SEAR OFF

POW:ALC:SEAR?

Notes

This command is accepted and does not raise an error.

ONCE is accepted, then value is restored to its previous value.

Preset

ON

State Saved

Yes

Choices

ON | OFF | ONCE

Initial S/W Revision

A.01.00

Power Search Immediate

Remote command only.

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SEARch:IMMediate

[:SOURce][:RF<channel>]:POWer:ALC:SEARch:IMMediate?

SCPI Example

POW:ALC:SEAR:IMM

POW:ALC:SEAR:IMM?

Notes

This command is accepted and does not raise an error. The Search query returns 0.

State Saved

No

Initial S/W Revision

A.02.00

Power Search Offset

Remote command only.

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce][:RF<channel>]:POWer:ALC:SEARch:OFFSet <rel_ampl>

SCPI Example

POW:ALC:SEAR:OFFS -10

Notes

This command is accepted and does not raise an error.

Preset 0

State Saved

No

Initial S/W Revision

A.02.00

Frequency and Phase

Tap or click within this area of the GUI to access the Frequency and Amplitude Adjustment Setup screen, where you can configure these parameters. Once you complete your configuration, click or tap Back and this area updates to reflect your custom configuration.

Frequency Mode

Remote command only.

Sets the frequency mode of the indicated channel.

CW: RF Output frequency is fixed to Frequency (CW).

LIST: RF Output frequency is controlled by List / Step Sweep settings.

SCPI Command

[:SOURce][:RF<channel>]:FREQuency:MODE CW|LIST

[:SOURce][:RF<channel>]:FREQuency:MODE?

SCPI Example

FREQ:MODE CW

FREQ:MODE?

Couplings
  • When Frequency Sweep State is set to OFF, and List/Step Sweep State is ON, Frequency Mode is set to CW.

  • When Frequency Sweep State is set to ON, and List/Step Sweep State is ON, Frequency Mode is set to List.

  • When List/Step Sweep State is set to OFF, Frequency Mode is set to CW.

Preset

CW

State Saved

Yes

Choices

CW|List

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:FREQuency:MODE

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:FREQuency:MODE FIXed to

[:SOURce]:RF1:FREQuency:MODE CW

Alias [:SOURce]: FREQuency:MODE SWEep to

[:SOURce]:RF1:FREQuency:MODE LIST

Alias [:SOURce][:RF<channel>]:FREQuency:MODE FIXed to

[:SOURce][:RF<channel>]:FREQuency:MODE CW

Alias [:SOURce][:RF<channel>]:FREQuency:MODE SWEep to

[:SOURce][:RF<channel>]:FREQuency:MODE LIST

Initial S/W Revision

A.16.00

Frequency (CW)

Controls the output frequency of the indicated channel.

When Vector Modulation is on, this is the center of the modulation frequency.

When Frequency List/Step Sweep is on, changing the frequency sets the Frequency List/Step Sweep off.

Do not use these SCPI commands for channel bonding. While an error or warning is not generated in this case, the fidelity of the bonded waveform is impaired.

Instead, refer to Frequency (CW) (Bonded).

GUI Location

RF Output > Frequency and Phase tab > Frequency (CW)

SCPI Command

[:SOURce][:RF<channel>]:FREQuency[:CW] <freq>

[:SOURce][:RF<channel>]:FREQuency[:CW]?

SCPI Example

FREQ 3 GHZ

FREQ?

Couplings

For M9484C with Option 8SG:

  • When Absolute Frequency Control is ON:

    • With only one signal enabled, changing the signal’s Absolute Frequency adjusts the RF Channel Frequency CW and vice-versa.

    • With more than one signal enabled for one RF channel, the RF Channel Frequency CW is adjusted as needed to contain all enabled signals at their specified Absolute Frequencies in the Modulation BW.

    • When turning a signal off , RF Channel Frequency is not adjusted in the cases other than single enabled signal.

Preset

1 GHz

When SCPI Backward Compatibility Mode is N51xxB:

- For Channel 1: Max

State Saved

Yes

Min

For M9484C = 9 kHz

Max

For M9484C:

  • With Option 506 = 6 GHz

  • With Option 508 = 8.5 GHz

  • With Option 514 = 14 GHz

  • With Option 520 = 21.6 GHz

  • With Option 532 = 31.8 GHz

  • With Option 544 = 44 GHz

  • With Option 554 = 54 GHz

  • With Option AL2 and V3080A-F06 connected = 67 GHz

  • With Option AL2 and V3080A-F07 connected = 75 GHz

  • With Option AL2 and V3080A-F09 connected = 90 GHz

  • With Option AL2 and V3080A-F11 connected = 110 GHz

Unavailable Range

For M9484C:

When Option AL2 and V3080A with any upconverter option connected:

  • With Option 532: 31.8 GHz < frequency < 52.8 GHz

  • With Option 544: 44 GHz < frequency < 52.8 GHz

Resolution

0.00001 Hz

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:FREQuency:FIXed

Backwards Compatibility Notes

For N51xxB:

  • Expand [:SOURce]:FREQuency:FIXed to [:SOURce][:RF<channel>]:FREQuency:FIXed

  • Alias [:SOURce][:RF<channel>]:FREQuency:FIXed to [:SOURce][:RF<channel>]:FREQuency[:CW]

Initial S/W Revision

A.01.00

Modified S/W Revision

A.03.00, A.07.00, A.09.00, A.11.00

History

Added the max value for Option F14/F20 at A.03.00

Added M1749A at A.07.00

Added M9484C at A.09.00

Added M9484C-AL2 and V3080A at A.11.00

Frequency (CW) (Bonded)

Sets the frequency directed to the Device Under Test; the signal at the output of the external combiner.

GUI Location

System Menu > Configure Channels > Bonded > Frequency (entry field)

SCPI Command

[:SOURce]:GROup<group>:CBONded:FREQuency[:CW] <freq>

[:SOURce]:GROup<group>:CBONded:FREQuency[:CW]?

SCPI Example

GRO:CBON:FREQ 18 GHZ

GRO:CBON:FREQ?

Dependencies

UP and DOWN are based on Bonded Frequency Increment Step

Preset

1 GHz

State Saved

Yes

Min

1 MHz

Max

For M9484C:

With Option 506 = 3.5 GHz

With Option 508 = 5.5 GHz

With Option 514 = 11.5 GHz

With Option 520 = 19.1 GHz

With Option 532 = 29.5 GHz

With Option 544 = 41.5 GHz

With Option 554 = 51.5 GHz

Resolution

0.01 Hz

SCPI Change

[:SOURce]:CBONded<bondingset>:FREQuency[:CW] <freq> has been changed to [:SOURce]:GROup<group>:CBONded:FREQuency[:CW] <freq>.

Prior use of :SOUR:CBON:FREQ or :SOUR:CBON1:FREQ is now :SOUR:GRO1:CBON:FREQ.

Initial S/W Revision

A.07.00

Modified S/W Revision

A.10.00 Changed SCPI: Added GROup<group> and removed <bondingset> from :CBONded

Frequency Increment

Remote command only.

Controls the incremental step value of the indicated channel for the Frequency CW or Fixed parameters. The value set with this command is not affected by *RST or a power cycle. It is reset to the default value with Restore System Defaults.

Do not use these SCPI commands for channel bonding. While an error or warning is not generated in this case, the fidelity of the bonded waveform is impaired.

Instead, refer to Frequency Increment (Bonded).

SCPI Command

[:SOURce][:RF<channel>]:FREQuency[:CW]:STEP[:INCRement] <freq>

[:SOURce][:RF<channel>]:FREQuency[:CW]:STEP[:INCRement]? [MAXimum|MINimum]

SCPI Example

FREQ:STEP 100 MHZ

FREQ:STEP?

Preset

This is unaffected by a Preset but is set to 100 kHz on a "Restore System Settings to Default Values."

State Saved

No

Min

0.00001 Hz

Max

99 GHz

Range

0.01 Hz to 99 GHz

Resolution

0.00001 Hz

Initial S/W Revision

A.01.00

Modified S/W Revision

A.09.00

History

Added M9484C at A.09.00

Frequency Increment (Bonded)

Remote command only.

Controls the incremental step value of the indicated bonding set for the Frequency parameters. The value set with this command is not affected by *RST or a power cycle, is it reset to default value with Restore System Defaults.

SCPI Command

[:SOURce]:GROup<group>:CBONded:FREQuency[:CW]:STEP[:INCRement] <freq>

[:SOURce]:GROup<group>:CBONded:FREQuency[:CW]:STEP[:INCRement]? [MAXimum|MINimum]

SCPI Example

GRO:CBON:FREQ:STEP 100 MHZ

GRO:CBON:FREQ:STEP?

Preset

This is unaffected by a Preset but is set to 100 kHz on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Min

0.02 Hz

Max

99 GHz

Resolution

0.02 Hz

SCPI Change

[:SOURce]:CBONded<bondingset>:FREQuency[:CW]:STEP[:INCRement] <freq> has been changed to [:SOURce]:GROup<group>:CBONded:FREQuency[:CW]:STEP[:INCRement] <freq>.

Prior use of :SOUR:CBON:FREQ:STEP or :SOUR:CBON1:FREQ:STEP is now :SOUR:GRO1:CBON:FREQ:STEP.

Initial S/W Revision

A.07.00

Modified S/W Revision

A.10.00 Changed SCPI: Added GROup<group> and removed <bondingset> from :CBONded

Fast Frequency

Remote command only.

Sets the instrument’s frequency with the maximum throughput.  As the purpose of this command is for speed, there is no limit checking, no coupling, and no update of the value on the front panel.  When using this command, there is no inclusion of frequency offset, multiplier, or frequency reference. The value is an integer frequency in 10 uHz resolution.  No error message is raised if the value is clipped.

SCPI Command

FAST<channel>:FREQuency <integer>

SCPI Example

FAST:FREQ 300000000000000

Notes

This command performs no coupling, does not support UP, DOWN, MIN, MAX, DEF.  The value is an integer in 10 uHz; no HZ, KHZ, MHZ, GHZ units are allowed.

State Saved

No

Min

Max

For M9484C:

  • With Option 506 = 600000000000000

  • With Option 508 = 850000000000000

  • With Option 514 = 1400000000000000

  • With Option 520 = 2160000000000000

  • With Option 532 = 3180000000000000

  • With Option 544 = 4400000000000000

  • With Option 554 = 5400000000000000

  • With Option AL2 and V3080A-F06 connected = 6700000000000000

  • With Option AL2 and V3080A-F07 connected = 7500000000000000

  • With Option AL2 and V3080A-F09 connected = 9000000000000000

  • With Option AL2 and V3080A-F11 connected = 11000000000000000

Resolution

10 uHz

Initial S/W Revision

A.14.00

Phase Transition Mode

Requires Option PCH.

This control selects the behavior of the phase across frequency changes.

Behavior with PCH Behavior without PCH

For Independent, Tx Coherent, and MIMO configurations, default is COHerent.

For Bonding configuration, default is RESet and not changeable.

Value is CONTinuos and not changeable

GUI Location

RF Output > Frequency and Phase tab > Phase Transition Mode

SCPI Command

[:SOURce][:RF<channel>]:PHASe:MODE CONTinuous|COHerent|UNDefined|RESet|MCOHerent

[:SOURce][:RF<channel>]:PHASe:MODE?

SCPI Example

PHAS:MODE CONT

PHAS:MODE?

Notes

For M9484C without Option PCH, the value is Continuous and not changeable.

Error message raised if user attempts to set value to HW that doesn’t provide it.

Only M9484C allows selection of MCOHerent.

Preset

With Option PCH: Coherent

Without Option PCH: Continuous

State Saved

Yes

Initial S/W Revision

A.09.00

Modified S/W Revision

A.11.00 - Added RESet selection, and created defaults appropriate to the selected configuration

A.15.00 - Added MCOHerent for M9484C

Phase

Controls the phase offset of the indicated channel.

With Option PCH, this parameter allows you to set the relative phase angle of each RF Channel relative to each other output.

When in "Tx Coherent" or MIMO, this parameter allows you to set the relative phase angle of the channels consumed by the Group relative to one another.

GUI units are degrees. SCPI return values are always in rad.

UP/DOWN increment is always 0.01.

GUI Location

RF Output > Frequency and Phase tab > Phase

SCPI Command

[:SOURce][:RF<channel>]:PHASe[:OFFSet] <angle>

[:SOURce][:RF<channel>]:PHASe[:OFFSet]? [MAXimum|MINimum]

SCPI Example

PHAS 30 deg

PHAS?

Notes

GUI units are degrees. SCPI return values are always in rad.

UP/DOWN increment is always 0.01

Wrap the value when it exceeds the limits.

Preset

0 deg

State Saved

Yes

Range

-180 to 180 deg

Resolution

0.001 deg

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:PHASe:REFerence

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:PHASe:REFerence to [:SOURce][:RF1]:PHASe[:OFFSet] 0

Initial S/W Revision

A.01.00

Modified S/W Revision

A.011.50 - Updated for M9484C.

A.18.00 - wrap the value when it exceeds the limits

A.20.00 - Added N51xxB Backwards Compatibility

Phase Reference

Remote command only.

Resets the phase of the RF output to zero.

SCPI Command

[:SOURce]:PHASe:REFerence

SCPI Example

PHAS:REF

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:PHASe:REFerence

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:PHASe:REFerence to [:SOURce][:RF1]:PHASe[:OFFSet] 0

Initial S/W Revision

A.20.00

Frequency Offset

Adds an offset value to the frequency of the indicated channel. The actual RF output frequency is not changed by this setting. The offset is applied after the Frequency Multiplier is applied to the frequency. When an offset has been entered, the OFFS indicator is turned on in the Frequency area of the display (top center of the display). The frequency offset state is turned on when any non–zero value is entered; entering zero will turn it off.

GUI Location

RF Output > Frequency and Phase > Frequency Offset

SCPI Command

[:SOURce][:RF<channel>]:FREQuency:OFFSet <freq>

[:SOURce][:RF<channel>]:FREQuency:OFFSet?

SCPI Example

FREQ:OFFS 100 MHz

FREQ:OFFS?

Preset

0 Hz

State Saved

Yes

Range

-200 to 200 GHz

Resolution

0.00001 Hz

Initial S/W Revision

A.01.00

Frequency Offset State

Remote command only.

Controls state of the Frequency Offset of the indicated channel. The state can be toggled between ON and OFF without affecting the value of the Frequency Offset.

SCPI Command

[:SOURce][:RF<channel>]:FREQuency:OFFSet:STATe ON|OFF|1|0

[:SOURce][:RF<channel>]:FREQuency:OFFSet:STATe?

SCPI Example

FREQ:OFFS:STAT ON

FREQ:OFFS:STAT?

Couplings

Setting Frequency Offset to 0 Hz turns this parameter OFF and setting Frequency Offset to any value other than 0 Hz turns this parameter ON.

Preset

OFF

State Saved

Yes

Choices

OFF | ON

Initial S/W Revision

A.01.00

Frequency Multiplier

Scales the frequency of the indicated channel by the specified value. The actual RF output frequency is not changed by this setting. The Frequency Multiplier is applied to the frequency prior to applying the Frequency Offset. When a Frequency Multiplier other than 1.0 has been entered, the MULT indicator is turned on in the Frequency Area (top center) of the display.

GUI Location

RF Output > Frequency and Phase tab > Frequency Multiplier

SCPI Command

[:SOURce][:RF<channel>]:FREQuency:MULTiplier <real>

[:SOURce][:RF<channel>]:FREQuency:MULTiplier?

SCPI Example

FREQ:MULT 2

FREQ:MULT?

Preset

1

State Saved

Yes

Range

-100 to -0.001 and 0.001 to 100

Min

-100

Max

100

Resolution

0.001

Initial S/W Revision

A.01.00

Modified S/W Revision

A.11.00 Change the min value from -1000 to -100, and max value from 1000 to 100

Frequency Reference On/Off

Enables or disables the frequency reference mode for the indicated channel. When Frequency Reference mode is on, subsequent frequency parameters are set relative to the reference value.

GUI Location

RF Output > Frequency and Phase > Frequency Reference On

SCPI Command

[:SOURce][:RF<channel>]:FREQuency:REFerence:STATe ON|OFF|1|0

[:SOURce][:RF<channel>]:FREQuency:REFerence:STATe?

SCPI Example

FREQ:REF:STAT ON

FREQ:REF:STAT?

Preset

OFF

State Saved

Yes

Choices

OFF | ON

Initial S/W Revision

A.01.00

Frequency Reference Value

Provides a reference frequency value for the indicated channel.

GUI Location

RF Output > Frequency and Phase > Frequency Reference

SCPI Command

[:SOURce][:RF<channel>]:FREQuency:REFerence <freq>

[:SOURce][:RF<channel>]:FREQuency:REFerence?

SCPI Example

FREQ:REF 3 GHZ

FREQ:REF?

Preset

0 Hz

State Saved

Yes

Range

-200 to 200 GHz

Resolution

0.001 Hz

Initial S/W Revision

A.01.00

Set Reference to Current Frequency

This immediate action sets the current CW output frequency, along with any offset, as a 0 Hz reference value to the indicated channel.

GUI Location

RF Output > Frequency and Phase > Set Reference to Current Frequency

SCPI Command

[:SOURce][:RF<channel>]:FREQuency:REFerence:SET

SCPI Example

FREQ:REF:SET

Initial S/W Revision

A.01.00

Optimizations

Tap or click within this area of the GUI to access the RF Optimizations screen. This area also displays the status of harmonic filters.

Optimizations pertain to the RF Output of the indicated channel. Each optimization may involve a tradeoff in one aspect of instrument performance over another. Care should be taken in choosing an optimization for your measurement use case.

List/Step Sweep

Refer to the topic List/Step Sweep.

Frequency List/Sweep

Frequency Center (Remote command only)

Refer to the section Frequency Center in Step Sweep Configuration.

Frequency Span (Remote command only)

Refer to the section Frequency Span in Step Sweep Configuration.

Frequency Start

Refer to the section Frequency Start in Step Sweep Configuration.

Frequency Stop

Refer to the section Frequency Stop in Step Sweep Configuration.

Corrections/De-embedding

RF Optimizations

List/Step Sweep